Dear Friends.Can someone explain the warning in the picture attached?If I change the "Clock and chip enable" parameters, the warning keep on.Best Regards.Thank you!
Dear friends.I am starting a new hardware designer for a project with the STM32H753 MCU.The project is a picture grabber and video recorder by infrared trigger. A display will be used to show the images/video using TouchGFX framework and the pictures...
ST6G3244MEBJR and TXS0206YFPR are clock limited at 60Mhz. The obsolete IP4856CX25 is 208MhzSo if I not wrong, you cannot use SDR50 and SDR104 bus speed modes.I have the same issue about the STM32H757 and Sandisk Extreme Pro card UHS-1.I would like to...
The reference manual says on page 1187 (DCMI Clocks): "The maximum DCMI_PIXCLK period must be higher than 2.5 HCLK periods."So, if AHB clock is 240 MHz / 96Mhz = 2.5Maybe is possible to work, but you are trying to use the DCMI interface in the max cl...