STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1578 Views
  • 0 replies
  • 2 kudos

Setting TIMER_TASK_PRIORITY with help of a macro

Hello @Khouloud ZEMMELI​ ,I have request with regards to TIMER_TASK_PRIORITY setting available under FreeRTOS -> Configuration Peripherals (with CMCIS V2 in use, which will set / Enable USE_TIMERS).I believe it is not a good practice to use a constan...

STM32F4 CubeMX codegeneration bug (RCC+LL)

STM CubeIDE 1.6.1STM32F411FW_F4 V1.26.1Driver LLNo string added when initializing date "RTC_DateStruct.Day = xx;"Details:https://github.com/STMicroelectronics/STM32CubeF4/issues/74#issuecomment-893317794

AAmik.1 by Associate
  • 1091 Views
  • 1 replies
  • 0 kudos

CubeProgrammer continually crashing

I am resuming electronics as a hobby after a significant hiatus.STM32Cube, MX and IDE are both fine. But the programmer is continually crashing.I am on linux and have replaced the OpenJDK by the Oracle JDK, no easy task for me either ! $java -version...

petereiso by Associate II
  • 2102 Views
  • 4 replies
  • 0 kudos

STM32L4R5ZI - Octospi bug in code generation

I am using the interfaces octospi1 and octospi2 to interface two qspi-nor flashes.The interfaces are configured the following way:Quad spi (octospi 1 uses low port 1 and octospi 2 uses low port 2)CLK (octospi 1 uses port 1 and octospi 2 uses port 2)N...

Seegras by Associate II
  • 1012 Views
  • 0 replies
  • 0 kudos