STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1568 Views
  • 0 replies
  • 2 kudos

Resolved! ADC Injected Mode LL code generation needs manual workarounds

I am using cubeIDE 1.5.0 with STM32F103RBTI configured 2 injected channels, triggered by Tim1 trigger out event in the device configuration tool. After thatcode generation for Initializing ADC injected group (call to function LL_ADC_INJ_Init) is comp...

FMink.1 by Associate II
  • 4488 Views
  • 9 replies
  • 0 kudos

Stm32cubeMx typo

It's not that disturbing and obviously it doesn't prevent anyone from using it, but it's years that you have "Search (Crtl+F)" instead of Ctrl in every search box.:grinning_face_with_sweat:

MFran.4 by Senior
  • 1996 Views
  • 4 replies
  • 0 kudos

Resolved! LL DMA Burst to a Timer not working on STM32H7

Hello,I am trying to use the DMA in burst mode to send data to a timer, to configure two PWM channels at every update event, but the DMA doesn't seem to write any data, however it doesn't trigger an error and triggers the transfer complete flag .I am...

MDega.2 by Associate II
  • 4957 Views
  • 4 replies
  • 0 kudos

Resolved! ADC DMA does not work

I m trying to configure the ADC1 in DMA modality with STM32F303K8when I debug the values does not change at all.With the breakpoint i could see that DMA1_Channel1_IRQHandler is called./* Private variables ---------------------------------------------...

FTrom by Associate II
  • 2027 Views
  • 4 replies
  • 0 kudos

Resolved! How do I enable MDMA_IRQHandler using STM32CubeIDE?

Hello there.I've setup simple transfer from SRAM4 to FMC NE1 on my STM32H750 board using MDMA. Write transfer itself complites, however no MDMA callbacks is ever called. After some digging i've found out that HAL_MDMA_IRQHandler is never called. On t...

BStud.1 by Associate II
  • 2145 Views
  • 2 replies
  • 0 kudos

LPUART + BDMA TX on STM32H730

I am attempting to use CubeMX to generate the code necessary to do a very basic demo of TX DMA using the LPUART and the BDMA peripheral (which as I understand it handles DMA for the LPUART1 which I'm using).Based on my reading of the reference manual...

AAG.1 by Associate
  • 2062 Views
  • 1 replies
  • 0 kudos