cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX / STM32CubeIDE100 - LWIP disabled (grayed out) - Solved

Jack3
Senior III

Using an STM32H753VIT I have configured the RMII peripheral for ethernet.

Now I also wanted to enable LWIP, but is is grayed out.

I am using the "Build-in" STM32CubeMX in STM32CubeIDE (1.0.0), on Windows 10.

There is no mention, why it is grayed out.

When I use the external STM32CubeMX (5.2.0), it is the same.

What can I check to enable LWIP?

UPDATE:

To make the LWIP selection possible, all I had to do is enabling the CPU caches (especially the DCache), which I had not done so far.

STM32CubeMX does not explain this.

Hope this helps somebody.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
GOtté.1
Associate II

Yes, it helped me for a NUCLEO-H743ZI2, thanks!

BPrin
Associate

Same here, gold. Thx a lot for sharing!!