STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1560 Views
  • 0 replies
  • 2 kudos

about stm32G070 TIM1

could a channel of TIM1 be configurated not only input mode but also output mode, so that it can capture a wave and generate PWM at the same time.

LOMO by Associate III
  • 1087 Views
  • 2 replies
  • 0 kudos

STM32F7 FMC SDRAM error after reinit

I have a custom board. There I have an issue with the FMC SDRAM after the HAL_SDRAM_Init call when calling it a subsequent(!!!) time. It works when doing the call the first time. I then deinit the SDRAM because of some current consumption tasks. When...

LFeld.1 by Associate
  • 2016 Views
  • 0 replies
  • 0 kudos

Resolved! HAL PWR Wakeup PINS do not match datasheet and cubemx.

Please tell me why the wakeup pin numbers are shifted up by one in the HAL PWR lib?See.. https://community.st.com/s/question/0D53W00001DKQdnSAH/wake-from-standby-not-working-stm32h753iit6?t=1637613024141If there is a legitimate reason for this mappin...

FColl.1 by Associate III
  • 3989 Views
  • 8 replies
  • 0 kudos

Resolved! I cannot use SW pins as GPIO for some reason

I swear i was able to do this in the past but then ...... then i updated from 6.3.0 to cubeMX 6.6.1.Maybe thats the reason, maybe not . Im using a stm32f105RBT6When i flash the chip and remove the stlink both PA13 and PA14 are stuck into some idle 1,...

0693W00000WJQkaQAH.png 0693W00000WJQhvQAH.png
Javier1 by Principal
  • 2730 Views
  • 5 replies
  • 0 kudos

If I want to make custom code structure or if I want to maintain 2 applications which have 2 different folders but can use same STM code, Is it possible? Can I change directory structure from cube MX or from any other tool?

If I want to make custom code structure or if I want to maintain 2 applications which have 2 different folders but can use same STM code, Is it possible? Can I change directory structure from cube MX or from any other tool? Like 2 applications which ...

AShah.10 by Associate
  • 1224 Views
  • 1 replies
  • 0 kudos

Cant change user labels for pins in cube 6.6.1

I tried to change the user label for multiple pins in Cube 6.6.1 running on a mac without luck. On the rare occasion where it takes the label, it ends up on the pin in the table reversed and you can't change it. For instance, I entered "TIM3" and ...