STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1578 Views
  • 0 replies
  • 2 kudos

Resolved! Where can I measure 25 megahertz intended for HSE?

STM32F407 Discoveryen.MB997-F407VGT6-C01_Schematic.pdfHSE quartz 8 megahertz.How are 4-26 MHz generated for HSE?With an oscilloscope, I see only 8 megahertz on X2 quartz.Where are those 25 megahertz that are listed as input for HSE?In the documentati...

_legacyfs_online_stmicro_images_0693W00000biD0jQAE.png
MMust.5 by Senior II
  • 1405 Views
  • 1 replies
  • 0 kudos

Resolved! How can I change the project name in STM32CubeMX

Hi,I have an issue, I can't change the project in STM32CubeMX. I wrote the project name V04 at the beginning of the project now I would like to change how can I do it. I don't touch even the textbox.Thank you

_legacyfs_online_stmicro_images_0693W00000biA5RQAU.png
BArsl.1 by Associate II
  • 3897 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F777ZIT FreeRTOS with Ethernet is not working.

Hello,We are struggling with the configuration of LwIP for my STM board over FreeRTOS.We have our own designed board with STM32F777ZIT controller.Ethernet and LWIP is working as expected as we used without FreeRTOS middleware but we are not able to i...

SKale1 by Associate II
  • 3785 Views
  • 4 replies
  • 0 kudos

Resolved! UART only receive one byte

I'm trying to receive more than 1 byte but it receive only 1 byte. Poll method or IT, it doesn't matter. Always receives 1 byte and writes it in rx_buffer[0]. When I search it I found out the reason is timeout, I increase timeout 1000 from 100ms but ...

MÇETİ.1 by Associate III
  • 12155 Views
  • 13 replies
  • 0 kudos

Resolved! HAL_I2C_Transmit returns HAL_BUSY.

I am trying to write a code so that I measure temperature and humidity via HTU21D sensor. It uses I2C interface. In the datasheet:The HTU21D(F) sensor requires a voltage supply between 1.5V and 3.6V. After power up, the device needs at most 15ms whil...

Resolved! Configuration of SDMMC peripheral in CubeMX

I am trying to connect to the WFM200 wifi module over SDIO. I am using the SDMM peripheral library/code for this.However, in the selection in CubeMX there is only the options for SD and MMC but no SDIO.Which option should I choose for using SDIO with...

0693W00000aITSEQA4.png
Hueli.1 by Associate III
  • 2352 Views
  • 2 replies
  • 1 kudos

STM32H7/F7 FMC Chip Selects

Hello,I'm looking for an MCU from the STM32H7/F7 lines that has the highest number of Chip Selects for the FMC bus. The highest CS count I've seen so far is the STM32H743:Is this the maximum 

_legacyfs_online_stmicro_images_0693W00000bhtcxQAA.png
skon.1 by Senior
  • 1943 Views
  • 2 replies
  • 0 kudos