STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1543 Views
  • 0 replies
  • 2 kudos

Resolved! STM32F7 Bug in CAN clock management

I work on a project with STM32F767ZI that uses 3 CAN buses and require them to be turned ON and OFF at specific times to save power.However, code generated by STM32CubeFW_F7 V1.16.1 (latest version at the time of posting) generates questionable(or ev...

SPI communication on STM32G4

OS : Ubuntu 22.04.2 LTSSTM32CubeIDE : 1.12.0 Build: 14980_20230301_1550 (UTC)Firmware : STM32Cube FW_G4 V1.5.1Working on interfacing Nucleo-G491RE to EVAL-AD5592R-PMDZ evaluation board using SPI interface (SPI2). Befor...

How do I get the USART to work on an STM32C011?

I am relatively new to using the STM32 family and I am trying to use the USART on a STM32C011J4M6 device without success.Initially I am just trying to send out a single character using the lines uint8_t TxData[] = {'@'}; HAL_UART_Transmit(&huart...

Neiliow by Associate III
  • 4762 Views
  • 7 replies
  • 0 kudos

CAN-Bus no callback/received frame; FDCAN STM32G474

Hello,when I try to receive a CAN-Frame it is not received by the Microcontroller, it is within the range, I have no idea what the issue is.Thanks to everybody in advance, Best Regards, Seppel  void FDCAN_Config(FDCAN_HandleTypeDef *pHfdcan) {   ...

0693W00000bhUdqQAE.png 0693W00000bhUe5QAE.png 0693W00000bhUeFQAU.png 0693W00000bhUf3QAE.png

Which class i have to choose in cubeMX configuration to communicate with FTDI USB, i didn't find Vendor Specific Class in the options ?

Insted of using the computer as the Host, i want to work with an STM32 microcontroller usb host. The device uses a standard FTDI USB to serial converter as the main mechanism to communicate between the computer and controller. Instead of using the co...

IChak.1 by Associate II
  • 1842 Views
  • 2 replies
  • 0 kudos

Resolved! how to set PPP with lte modem

I am testing LTE modem with a STM32H747 MCULTE modem is connectied with STM32H747 thru USART2.I want to use PPP communications with LTE modem.but when I try to check LWIP in [Pinout & Configuration] of IOC file,I can't set [Enabled] of [LWIP Mode and...

Resolved! ADC LL drivers for L4

MX generated ADC drivers like this: /** Configure Regular Channel */ LL_ADC_REG_SetSequencerRanks(ADC1, LL_ADC_REG_RANK_1, LL_ADC_PATH_INTERNAL_VREFINT); LL_ADC_SetChannelSamplingTime(ADC1, LL_ADC_PATH_INTERNAL_VREFINT, LL_ADC_SAMPLINGTIME_247...

WQ by Associate III
  • 1518 Views
  • 1 replies
  • 0 kudos