STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1568 Views
  • 0 replies
  • 2 kudos

Option/feature suggestion - Discussion CubeMX

I had changed a library file, and i wondered, why after a MX config generation it did not work anymore.CubeMX replaced all the files!!! Lucky i had some backup. Why would you replace library files, that were already copied? Please see my picture for ...

Tobe by Senior III
  • 4078 Views
  • 7 replies
  • 1 kudos

Resolved! Problem with CubeMX after upgrading - can't open ioc file

I upgraded STM32CubeIDE to 1.14.0 and then when I went to open an ioc file I got this message:This project was setup with STM32CubeMX V6.9.2 using STMCube FW_G0 V1.6.1.There are two options to proceed:-Migrate:Migrate your project using the current S...

Dabbo by Associate III
  • 10428 Views
  • 10 replies
  • 0 kudos

SDCARD does not work with 4bits wide bus

Hi I have STM32F407 and after updating STM32CubeMX 6.6.1 -> 6.9.2 I faced the same issue with SD card:https://community.st.com/t5/stm32cubemx-mcus/sdcard-does-not-work-fr-not-ready-when-migrating-from-fw-f4-v1/m-p/115499#M3876It seems that with previ...

JBond.1 by Senior
  • 8450 Views
  • 8 replies
  • 2 kudos

Resolved! How Ethernet MAC interrupts have been enabled by STM32CubeH7?

Hi all. This is the first time I am using CubeH7 + FreeRTOS + LwIP. I have tried to trace down how Ethernet MAC interrupts have been enabled. If I got the code correctly:+ I enabled "Ethernet global interrupt" option from CubeMX "ETH".+ I enabled "Lw...

Leon_MS by Associate III
  • 2666 Views
  • 2 replies
  • 0 kudos

problems with STM32F405 SD Card 4wiresCubeMX

hello,i work in STM32F405, create projet with cubeMx, SD 4 wires.Pull up in the schematic D0..3 , CMD, no internal pull in cube MXmount return FR_NOT_READYwhen SD_WideBus_Enable() (in hal_sd) call:in SD_FindSCR() after the cmd 51 , there is a polling...

trave.1 by Associate II
  • 3343 Views
  • 3 replies
  • 2 kudos

Resolved! How to debug dual core simultaneously in mdk arm

Hi every body.I have a project with stm32h747aii and i use mdk arm. Recently i did it with cubeide and i could debug both cores at the same time and within one window.I wanted to know that if it is possible in mdk arm 5.36 or not?When i enter each co...

ArmanIlmak_0-1701851987312.png