STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1628 Views
  • 0 replies
  • 2 kudos

Resolved! STM32H573VITxQ RMII interface

I'm planning to build a low-power Ethernet project using the STM32H573VI microcontroller. I need to use an SMPS to lower power consumption because of that reason i choose that MCU. During createation of project, I noticed that STM32CubeMX offers RMII...

alpkra by Associate
  • 3296 Views
  • 4 replies
  • 2 kudos

Problems with CubeMx 6.12 + adc5 + dma

In my project I use 4 adc, managed with the same code. With adc5, and two channels, I had a problem: I read two equal values, that is, the second was equal to first channel.After several searches I discovered that, in the adc.c file created by cubemx...

STM32CubeMX 6.12 deletes user folder

Hi, When I'm generating code with the latest STM32CubeMX 6.12.1 and STM32CubeIDE1.16.0  then sometimes my user folder with the include files were deleted. I don't know yet, why sometimes the folder is not deleted (maybe only small changed in the .ioc...

nobody by Associate II
  • 2585 Views
  • 6 replies
  • 0 kudos

Bug in X-Cube-AZRTOS-H7 V3.3.0

Hello STM-Team,I'm working on my project with an STM32H723ZG and ran into an issue with the code generation when I selected "Network Interfaces" in the  AZRTOS configuration.The code generation will add "NX_ETH_INTERFACE_ENABLED" to the "RTE_Componen...

Intector_1-1733095953265.png Intector_2-1733096278529.png