[Bug report] Cube MX doesn't generate Open drain for PWM channels
This bug was in previous version (old user interface) and present in new versionThere are not initialization in MX_GPIO_Init(); and in MX_TIM3_Init();
This bug was in previous version (old user interface) and present in new versionThere are not initialization in MX_GPIO_Init(); and in MX_TIM3_Init();
STMCubeMX V 5.0 MCC STM32F413VHT6, TIM6 problem I'm using LL libraries. The interrupt generated with any setting always has a frequency around 3.6 MHz. Thanks for your help.
Hi. I'm KAI. I want to configure the system to receive the sensing value by ADC.The system configuration I am currently thinking is as follows.The system is the same as the attached file. In STM32F103RB, the serial data and the SR clock signal are in...
I was trying to write a code to integrate a input signal, triggering the ADC with a timer, and print the information every 0.5 s with the systick. I don't understand why After the first saturation of the timer, the code doesn't enter in the systik ha...
Posted on September 09, 2017 at 06:39Update: As the below error appeared when I tried to make a Low Layer project for Nucleo L152RE board using STM32CubeMX in generating a code for a Makefile project, and, it was solved by an update to both STM32Cub...
I'm using an STM32F030K6 and I need to measure the time between the rising edge of 2 signals.The 2 signals (square wave) are not in phase and intended to use TIM1 to:* rising edge of signal 1, make timer start (internaly clocked);* rising edge of sig...
I need to get data from 2/4 regular channels of ADC1 at every TIM4_CC4 event and save it with DMA. But always every time I receive ADC OVR error.When I start ADC with HAL_ADC_Start_DMA I receive 1 immediate conversion with transfer. Then I start TIM ...
Hello everyone,I have problem with my univeristy project and I'm trying to find some help.I'm using Nucleo64 STM32F411RE.The most important setting in CubeMX:In ADC every rank have 3 cycles, and Rank 1-4 Channel 10, Rank 5-8 Channel 11, Rank 9-12 Cha...
Hello, I can`t figure out how to achieve the following with STM32Cube HAL.I need to setup a timer, that counts to a specific value and generate an Interrupt. After this, the timer needs to keep counting up, until it overflows. This Overflow should al...
Let's take example STM32F407 MCU TIM3_CH1 timer is configured for indirect capture mode meaning this channel is triggered by TIM3_CH2 input signal. In this mode TIM3_CH1 external pin is not used. Can it be configured as this channel' output? If yes, ...