User Activity

Posted on August 18, 2017 at 08:34Hi,I'm using custom hardware that has STM32F303VB (firmware version F3 v1.8.0) and uses USB in self-powered mode.I have modified USB Custom HID class to appear as USB Vendor Class (1 IN + 1 OUT endpoint). USB Vendor...
Posted on August 04, 2017 at 08:19Hi,I'm working on my custom hardware based on STM32F303VBI'm trying to make a CAN based boot loader. I can jump from boot loader to application but the application just hangs some where.How can I debug boot loader +...
Posted on July 31, 2017 at 15:36Hi,I'm using STM32F303VB in my custom hardware that requires boot loading STM32 over CAN. I'm writing a CAN boot loader.I want to know, how to switch/jump from boot loader to application?Is there any document or proje...
Posted on June 14, 2017 at 12:20Hi,I'm using STM32F303VB in my custom hardware that has USB.When using STM32CubeMX I see a lot of Standard USB Device classes that I can use (Audio Class, HID, Custom HID,.. etc..). But I do not see an option for Vend...
Posted on June 13, 2017 at 14:59Hi,We are using STM32F303VB on our custom hardware. We plan to use the STM32 as a USB device talking to a PC (USB Host).(I'm using STM32CubeMX (STM32Cube_FW_F3_V1.8.0) to generate project for AC6 System Workbench.)I h...
Kudos from