User Activity

STM32CubeIDEVersion: 1.12.1Build: 16088_20230420_1057 (UTC)I am trying to use one of the examples from the STM32Cube_FW_WB0_V1.1.0 package, but I am unable to build any of them.After importing the project into STM32CubeIDE (I have tried BLE_Beacon an...
Posted on June 10, 2016 at 11:39 Hello, I noticed that the STM32CubeMx doesn't generate default struct initialization in the code. This doesn't usually raise an error because all fields are tipically initialized, but sometimes this doesn...
Posted on June 08, 2016 at 16:48Hi, setting the ADC1_IN8 or ADC_IN15 as OPAMP x Output Differential  or OPAMP x Output Single-ended in STM32CubeMx v 4.15 with NUCLEO-L476RG doesn't generate the correct GPIO setup. The OPAMP output pins are configur...