STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1606 Views
  • 0 replies
  • 2 kudos

STM32CubeMX 4.25 STM32L433RCTx SystemClock_Config Bug PLLM

Posted on April 11, 2018 at 11:48Hi guys.I'm working in a STM32L433RCTP based project.The code generated by the Stm32CubeMX for clock configuration has no value set for the PLL-M prescaler in the  PLL struct, see original code:----------------------...

H. K. by Associate
  • 2948 Views
  • 7 replies
  • 0 kudos

STM32F103 Timer Interrupt Issue

Posted on September 07, 2017 at 13:48Hello, I'm using STM32F103RBT6 for my project, I've designed a custom board. I'm using cubemx to generate the basic code and Atollic for debugging.I'm reading the switches using external interrupt. In the externa...

[BUG] STM32F4 SDIO and CMSIS driver MCI interface

Posted on April 02, 2018 at 17:41Hello ST,I found that code, generated by STM32CubeMX for STM32F4 SDIO periperal, is poorly integrated with MCI interface (CMSIS driver). And doesn't work out of box without modification.STM32CubeMX generates HAL_MMC_...

0690X0000060AIoQAM.png
Eugene S. by Associate III
  • 2175 Views
  • 3 replies
  • 0 kudos

cumbeMx update error

Posted on April 26, 2018 at 12:05 when i tried to update the cube mx and also installing cubemx for F7 , i encountered this error . please help how to solve this . screenshot is attached. Thanks. #stm32-cubemx

0690X0000060AnHQAU.png
n.serina by Associate III
  • 887 Views
  • 1 replies
  • 0 kudos

STM32L1 I2C register read problem

Posted on April 24, 2018 at 13:58Hi, I have for me big problem with I2C. I would like communicate with DS3231 RTC chip.I wroted small easy code :void DS3231_DateTime_get(void){ DS3231.ds3231_TX_buff[0] = 0x00; HAL_I2C_Master_Transmit(&hi2c1, DS3231_...

0690X0000060AlQQAU.png 0690X0000060AlVQAU.png
lorant124 by Associate III
  • 853 Views
  • 2 replies
  • 0 kudos

STM32L4R9 CubeMX - SDMMC + DMA

Posted on March 26, 2018 at 14:29Hey, i tried to setup my STM32L4R9 with CubeMX v4.25.0 as followed:- FreeRTOS- FatFS- SD Card- DMA Support unfortunately i noticed that the DMA-Interrupt tab does not show up in the SD-Card settings. I tried it with ...

STM32L1 SDIO

Posted on April 23, 2018 at 12:41Hi, I would like use SD card with SDIO 1bit, FatFS.I tried to wit cubemx 4.17 on F407, it is worked good.But I would like to use with STM32L151RD.I tried with CubeMX 4.25 FW 1.8.1, FatFS R0.11.But doesnt work anythin...

lorant124 by Associate III
  • 955 Views
  • 1 replies
  • 0 kudos

Pwm input capture mode in stm32H7 MCU

Posted on April 22, 2018 at 05:41HELLO..I want to measure the frequency and duty cycle of the external signal. I have gone through some example available , and suggestions on website. Everywhere they are using either channel 1 or channel 2 in any of...

1588 PTP on STM32F746ZG

Posted on April 13, 2018 at 11:06hey,I have a LWIP client/server application and I want to add the PTP synchronization feature to the communication. I'm using STM32F746ZGTx Nucleo and CubeMX. I'm trying to enable RMII_PTP_Synchro mode for ETH (after...