STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1586 Views
  • 0 replies
  • 2 kudos

Resolved! STM32CubeMX issues with STM32H743ZITx

I tried to use the STM32CubeMX to configure DAC to work with DMA which would enable me to transfer data from memory, all clocked by TIM6. I used same configuration for STM32F334 and it worked without any problems. After I never got this working, I tr...

0690X0000060R5tQAE.png
RichardS1 by Associate II
  • 1900 Views
  • 3 replies
  • 0 kudos

CubeMX and One Pulse Mode

Posted on September 28, 2017 at 11:49In STM32CubeF4 STM32F446ZE, there is a timer one pulse mode example.Setting TIM3 CH2 as input capture and CH1 as Output Compare to work as One pulse mode.(Set slave mode as trigger mode and trigger source as TI2F...

0690X00000602UmQAI.bmp 0690X00000602V0QAI.bmp
Zt Liu by Senior III
  • 2170 Views
  • 1 replies
  • 1 kudos

LIN Transmit Message

Hey there i want to send and receive LIN Message through my MCU (STM32F091CCT6 - TJA1021T/10/C LIN Transreceiver). But i cant see any example code in documents.Here what i did for this.I select USART1 in LIN mode and USART2 Asynchronous mode to see ...

Resolved! Idea needed for 9 bit spi transfer using HAL Library

Posted on January 18, 2017 at 03:55I am using stm32cubeMx to generate initialization C code for programming STM32L476RGTx MCU using Keil IDE. Recently, I need to interface an AD5262 digital potentiometer to control the gain of an amplifier automatic...

STM32F4 DISCOVERY + SDIO 1BIT + MDK 5 ISSUE

Dear All, I am working with STM32F4 Discovery board. I have been stuck with the sd card interface for last 1 week. I have used cubemx version 4.26 for creating this project. But F_mount function is not working.Please find the below code. and kind...

Yadav by Associate II
  • 1126 Views
  • 1 replies
  • 0 kudos

STM32CUBEMX Ver 4.26.1 horrific bug

Something has change with Version 4.26(.1)Any time I look at the Project Settings (even with no changes) I get a message saying:"This Project File (System.ioc) already exists in the chosen folder. Overwrite this file by this new Project?"If I say No ...