User Activity

I'm curious what is the best way to debug a User Application when using SBSFU on a STM32.Of course the security mechanisms in SBSFU/SECore must be disabled to allow debugging at all and basically just downloading the UserApplication and debug it with...
The latest version of the STM32CubeMX 4.27.0 deletes empty folders in my project structure during project generation.This is a nice feature if it deletes only previously generated folders that are not used any longer, but it also deletes folders that...
Posted on February 19, 2018 at 10:22Dear Team,I've migrated my CubeMX project for a STM32F412 MCU today and there are some changes which I would classify as bug.1) I've configured TIM6 as System-Timer (Timebase-Source) in the SYS-category. Since V4....
Kudos from
Kudos given to