STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1674 Views
  • 0 replies
  • 2 kudos

Upgrade issues from 4.27 to 5.2

We have been having issued with printf redirection on more recent Cube versions, so I got out on eval board and built a Hello World project.I created it with CubeMX 4.27, got it working (seems ?default? libraries at some point, as I had to change __i...

STM32F407VGTx / CDC / Error Driver

Hello,I test the CDC with my STM32F407VgTx in an up-to-date environment: Windows 10 / STM32CubeMx v5.20 / SW4STM32 / System WorkBench for STM32/ST-LINK V2The VCP v 1.50 driver for windows 10 has been installed normally and declared active.The source ...

CC_ROB by Associate II
  • 23455 Views
  • 29 replies
  • 0 kudos

Resolved! NVIC PRIO BITS could not be resolved - [Solved]

Hi to everybody, I am a total mcu beginner and I cannot compile a project. I did not write a single line of code, just tried to build. When I tried to do it I had 12 identical errors.What can I do? I have a STM32 F446RE Nucleo 64 board, Cube MX 5.1.0...

0690X000008wTJnQAM.jpg
AMoro.4 by Associate II
  • 3170 Views
  • 5 replies
  • 0 kudos

stm32f407 virtual com

on the win10, the stm32cubemx generated project does not work, i do not know what's the errorint main(void) { /* USER CODE BEGIN 1 */   /* USER CODE END 1 */   /* MCU Configuration--------------------------------------------------------*/   ...

0690X000008a7eMQAQ.png

Where are all the examples that came with CubeMX?

Coming from a short odyssey with CubeMX and System Workbench, I just installed STM32CubeIDE. I decided so 'cause I had quite some issues in copying projects from the examples provided in the CubeMX installation and thought STM32CubeIDE would be a com...

TLaue by Associate
  • 1435 Views
  • 2 replies
  • 0 kudos

Resolved! STM32L011 Temperature sensor calibration (Possible bug in library)

Hi all, I am trying to use internal temperature sensor on Nucleo L011K4 and using macro from LL library (__LL_ADC_CALC_TEMPERATURE_TYP_PARAMS) I get complete garbage. STM32Cube_FW_L0_V1.11.2STM32CubeMx 5.0.1LL libraries used, no HALADC is running in ...

EPopr by Associate II
  • 7379 Views
  • 10 replies
  • 0 kudos

Monitor DPI problem

Is there any workaround that I can use to solve the issue regarding the super tiny font size with the ioc editor. It is actually quite difficult to work with at the moment given my laptop screen resolution is 3000x2000.

Why .json files can not be downloaded?

I use windows 10 and stm32cubemx and when i try to start a project by choosing a board selection it shows me errors downloading *.json files (mcusdocs.json, ...)I deleted the .stmcufinder .stmcube .stm32cubemx directories but no effect!

0690X000008wL6gQAE.jpg
radikv by Associate II
  • 6163 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.