STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1568 Views
  • 0 replies
  • 2 kudos

Resolved! STM32CubeMx can't load project - freeze

hi.When I try to open the project file, it does not respond and it does not go any further.Perhaps this is happening since the update.​attaching debug information, please confirm.​​

HJung.6 by Associate II
  • 1623 Views
  • 2 replies
  • 0 kudos

Upgrade issues from 4.27 to 5.2

We have been having issued with printf redirection on more recent Cube versions, so I got out on eval board and built a Hello World project.I created it with CubeMX 4.27, got it working (seems ?default? libraries at some point, as I had to change __i...

STM32F407VGTx / CDC / Error Driver

Hello,I test the CDC with my STM32F407VgTx in an up-to-date environment: Windows 10 / STM32CubeMx v5.20 / SW4STM32 / System WorkBench for STM32/ST-LINK V2The VCP v 1.50 driver for windows 10 has been installed normally and declared active.The source ...

CC_ROB by Associate II
  • 22290 Views
  • 29 replies
  • 0 kudos

Resolved! NVIC PRIO BITS could not be resolved - [Solved]

Hi to everybody, I am a total mcu beginner and I cannot compile a project. I did not write a single line of code, just tried to build. When I tried to do it I had 12 identical errors.What can I do? I have a STM32 F446RE Nucleo 64 board, Cube MX 5.1.0...

0690X000008wTJnQAM.jpg
AMoro.4 by Associate II
  • 3081 Views
  • 5 replies
  • 0 kudos

stm32f407 virtual com

on the win10, the stm32cubemx generated project does not work, i do not know what's the errorint main(void) { /* USER CODE BEGIN 1 */   /* USER CODE END 1 */   /* MCU Configuration--------------------------------------------------------*/   ...

0690X000008a7eMQAQ.png

Where are all the examples that came with CubeMX?

Coming from a short odyssey with CubeMX and System Workbench, I just installed STM32CubeIDE. I decided so 'cause I had quite some issues in copying projects from the examples provided in the CubeMX installation and thought STM32CubeIDE would be a com...

TLaue by Associate
  • 1389 Views
  • 2 replies
  • 0 kudos

Resolved! STM32L011 Temperature sensor calibration (Possible bug in library)

Hi all, I am trying to use internal temperature sensor on Nucleo L011K4 and using macro from LL library (__LL_ADC_CALC_TEMPERATURE_TYP_PARAMS) I get complete garbage. STM32Cube_FW_L0_V1.11.2STM32CubeMx 5.0.1LL libraries used, no HALADC is running in ...

EPopr by Associate II
  • 7203 Views
  • 10 replies
  • 0 kudos