STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1591 Views
  • 0 replies
  • 2 kudos

How to read ADC with Dual Regular + Differential mode?

Hello!I have found a lot of examples about simple ADC reads, with:-single channel single conversion-single channel continuous conversion-multi channel single conversion-multi channel continuous conversionAnd these with polling, interrupt and DMA.I ne...

SFeje by Associate II
  • 1819 Views
  • 1 replies
  • 0 kudos

STM32H743 raw LwIP ping - not working

Hi everyone,I have an STM32H743 Nucleo kit with ethernet interface. I'm trying to make alive a simple TCP/IP demo with the raw LwIP stack. I'm using STM32CubeMX with TrueStudio.In the Cube I have configured the followings:- Clock is set to th highest...

Attila by Associate II
  • 1844 Views
  • 2 replies
  • 0 kudos

Resolved! About flash size of STM32H743

About STM32H743VGT6Selector of STM32CubeMX show that flash size of STM32H743VGT6 is 1024K.but when i used STM32CubeProgrammer to connect it,that show flash size if 2048K。even the sector from 0x0810 0000 to 0x081f ffff can be erase and program to。so t...

csinu by Associate II
  • 2052 Views
  • 1 replies
  • 1 kudos