User Activity

Dear ST technical supportI'm working with a temperature sensor TMP102 and NUCLEO STM32F767ZI with I2C communication mode. CUBE v5.6.0 and firmware STM32F7 1.16.0, and SW4STM32.Well, I started to read the sensor and I tested the next commands:HAL_I2C...
Dear technical support I'd like to notify you that seems that there is an error in you CUBE version 4.24 until the latest one 5.1 (i checked one by one and there is an error with the DMA RX in circular) Before (with previous CUBE versions) I was usin...
Posted on May 02, 2018 at 18:02I have the next error in the command window of Matlab 2018a''TIMERS_Config function : Can not find which APB timer TIM1 is connected to.Default preference value STM32TIMAPB set to APB1 is used.''Hello community! first,...
Posted on November 14, 2017 at 12:28Hello ST teamI'm writing to you because I'm working onSTM32F746ZGTx, but I have found the same BUG problem with the SD card in CubeMx version 4.23.0 library Firmware package STM32F7 v1.8.0.Before I was working wit...
Kudos from