STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1591 Views
  • 0 replies
  • 2 kudos

Resolved! I2C clock configuration issue on STM32F746ZG

I've been working with I2C on STM32s for some time and I noticed an issue while probing my signals with an oscilloscope.I set my project with CubeMX and usse Atollic TrueStudio as an IDE. Everything works fine. However, I've noticed that the real fre...

t.poncot by Associate II
  • 6939 Views
  • 9 replies
  • 0 kudos

STM32L4S9 locked by cube programmer?

Hello, I am facing some strange behavior when I try to debug a stm32l4s9 MCU using Atollic TrueStudio 9.3.0.When I try to debug the mcu using a st-link v2 I get following output:STMicroelectronics ST-LINK GDB server. Version 5.1.0 Copyright (c) 2018,...

0690X00000AQncgQAD.png 0690X00000AQndTQAT.png
CKren by Associate
  • 1285 Views
  • 1 replies
  • 0 kudos

bxCAN acceptance filter configuration.

Hi,I'm using CubeMX to init CAN module, everything is working, I can send and receive messages.Now I would like to configure filter to accept only message with specified ID.So, I have this piece of code generated by CUBE: //sFilterConfig.FilterNumber...

DKarc by Associate II
  • 1453 Views
  • 1 replies
  • 0 kudos

Resolved! How do I generate a BSP that CubeMX will recognize?

The FatFS library references a BSP function to determine if a SD card is plugged in. Since I don't have a BSP for this PCB, CubeMX complains about the missing function. How do I generate a BSP that CubeMX will recognize to eliminate this configurat...

GJohn by Associate II
  • 1441 Views
  • 2 replies
  • 0 kudos

STM32L452 usb support in IDE generation?

Hi.I am trying to add usb CDC to a project for the STM32L452 mcu. Project can be created, compiled without problem.I did a test with a simple and non-modified project that just had the usb added. To my despair, machines do not see the device and no e...