User Activity

If I try to configure the interface from the CubeMX tool, it seems that it is possible to communicate only with flash memories.I have a lot of data that I need to transfer from a uC to another on the same PCB and a single SPI is too slow. Are there o...
Hi,I am not able to connect NUCLEO-L4P5ZG board to a PC and ST_LINK utility. It alway gives me "unexpected error". Detailed message follows:15:06:46 : ST-LINK SN : 066BFF343039564157205441 15:06:46 : ST-LINK Firmware version : V2J35M26 15:06:46 : Con...
For example if the original name is:void HAL_GPIO_Init(GPIO_TypeDef *GPIOx, GPIO_InitTypeDef *GPIO_Init);the expected result should be:void MyPrefix_HAL_GPIO_Init(GPIO_TypeDef *GPIOx, GPIO_InitTypeDef *GPIO_Init);
Kudos from
Kudos given to