STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1574 Views
  • 0 replies
  • 2 kudos

STM32CUbe MX db files usability in an external tool(s)

I started small project, where I use "db/plugins/clock" XML file(s) from CubeMX to visualize the state of the clock-tree in the running STM32.Currently I face number of issues. Mybee you can direct me to other resources more suitable than CubeMX file...

UART4 Unavailable on STM32F750N8-DK?

I want to use only the Tx pin on UART4, it is on PA0/CN5-1 of the Arduino connector. I setup// Initialize UART4 for Debug Terminal 250 kbaud using 50 MHz PCLK1 /////////////////////////////////   PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHC...

DRobe.4 by Senior
  • 1488 Views
  • 3 replies
  • 0 kudos

Resolved! stm32h7 dtcm ram overflowed

Hello, I am relatively new in this field, and need assistance for my project at work.Recently, in order to have more RAM, I switched from STM32F4 to STM32H7. I saw that STM32H7 has 1MB of RAM, and decided to base our system on this MCU. However, afte...

VYoun by Associate III
  • 7759 Views
  • 13 replies
  • 0 kudos

Resolved! about RTC calibration! by use for LSI clk. (STM32F091V)

I use STM32F091VI use LSI for RTC clock.I know that LSI is inaccurate.I set the RTC interrupt to 1 second.However, the interrupt interval was 860ms.Can anyone tell me how to calibrate the RTC?I am happy with the sample source code.

Ukazu by Associate III
  • 2032 Views
  • 4 replies
  • 0 kudos

Resolved! STM32H7 SDMMC STMCubeMX firmware 1.6.0 FATFS

Hello,I am total new to this field and need your help please. I have an application in which I measure data and collect in a matrix on ram. after the measurement is finished, I write the data on SD card and USART. I had a code that worked perfectly o...

0690X00000DBuhtQAD.png 0690X00000DBuhyQAD.png
VYoun by Associate III
  • 2216 Views
  • 4 replies
  • 0 kudos

Resolved! CubeIDE deletes files. What am I doing wrong?

I've got an issue with the CubeIDE from STM (Version 1.1.0). I generated a Cube project, worked with it for 2 months, edited it,... no major problems. But suddenly the IDE deletes files like my main.cpp,.. I just did some adjustments, like adding ano...

MWetter by Associate III
  • 3256 Views
  • 7 replies
  • 0 kudos