STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1568 Views
  • 0 replies
  • 2 kudos

Possible Bug in cubeMX 5.6.1

Not really an issue, but it is worth mentioning...inside cubeIDE, i generate a new stm32 project, in target selector i select the nucleo f446re board and initialize it with the standard peripheral settings. When checking the clock configuration, i wo...

chaaalyy by Senior II
  • 1160 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F446: bug when using DMA UART

We wanted to use a UART periphal in transfer DMA mode. When configuring it with CubeMX, nothing happens, event when trying it on an empty project.When manually configuring the various registers for DMA transfer between memory and the peripheral data ...

THerp.1 by Associate II
  • 1937 Views
  • 4 replies
  • 0 kudos

No SPI MOSI and CLK without NSS?

I don't need NSS signal or pin, I would rather use it as a real Chip select. But it looks like it there is no SPI at all without NSS? What should I change? CPU is STM32H750.Edit: Where did my screen capture go? For a short while I thought that I coul...

0693W000000Wfo1QAC.png
LMI2 by Lead
  • 3332 Views
  • 7 replies
  • 0 kudos

STM32H745 Inter core data transfer

 have periodic tasks (with period set by timer interrupts) running on both cores and i want to exchange data between cores. Here is a simple example.. M7-- Does some calculations and generates a variable at 20KHz M4-- Has to use the above variable fo...

Madhan by Associate II
  • 2367 Views
  • 4 replies
  • 0 kudos

Unable to install CubeL4 version 1.15.1 (patch) in CubeMX

Running CubeMX version 5.6.1 on Win10. No internet connection, so I manually copy the CubeL4 zip files to the PC and then try to install via the "Install/Remove" button under software packages. I have CubeL4 1.15.0 installed. When I check 1.15.1 a...

Bob S by Super User
  • 2862 Views
  • 1 replies
  • 0 kudos

H743 - SWO not working - PB3 floating

I still struggle with SWO on a custom board with two H743s on it. No matter what I try, SWO pin PB3 is floating. I could get the SWO of a H743 Nucleo board with the hack of clive1 in this post below work a few years ago, but with current firmware/Cub...

CKosa by Associate II
  • 2036 Views
  • 0 replies
  • 0 kudos