STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1568 Views
  • 0 replies
  • 2 kudos

CubeMX USB RTOS issue

      在32位中,字的单位应该要*4吧?为什么这里直接是按字节赋值???坑死我了 Translation: "In 32-bit, the word unit should be * 4, right? Why is it assigned directly by byte here? ? ?"   Edited by ST moderator to be inline with the community rules. In next time please write in E...

dxgvbsdfgsd_0-1756272017129.png dxgvbsdfgsd_2-1756272037356.png dxgvbsdfgsd_3-1756272048683.png dxgvbsdfgsd_4-1756272140038.png

Resolved! STM32_WPAN is grayed-out in MX

Dear STMicroelectronics Support Team,I hope this message finds you well.I am currently working with an STM32WB series microcontroller and using STM32CubeMX (version [insert version number]) for configuration.While setting up the project, I noticed th...

Bug report - HRTIM ADC Trigger post scaler STM32G474

HelloHRTIM´s ADC Triggers post scalers on STM32G474 have 5 bits (0..31) , but in CubeMX you can set 10 bits (0..1048575). Upper bits are trimed so it can be confusing when you set value above 31. My versions:STM32CubeMX Version: 6.15.0-RC7 Build: 202...

PDvor.2 by Associate
  • 414 Views
  • 2 replies
  • 0 kudos

No code when IO Pin Swap enabled

When I select IO pin swap in CubeMX, the LL SPI initialization code does not update the pin swap register.Using H5 Nucleo board and LL HAL.  Easy workaround if you know to look for it. 

Stephen9 by Associate II
  • 716 Views
  • 3 replies
  • 2 kudos

CubeMX not generating code

Hello all, I recently install CubeIDE and I want to do a blinky example on the User led for the nucleo-U545REI see that the GPIO for the USER LED is PA5 So in cubeIDE, I open CubeMX, configure PA5 PIN TO GPIO_OUTPUT and try to generate the code by cl...

2345.png
estora by Associate
  • 7341 Views
  • 9 replies
  • 2 kudos

Resolved! STM32CubeMX 6.15.0, STM32H523CET6, TouchGFX

When the TouchGFX Graphics Application is selected, the supplementary TouchGFX code is generated; however, the TouchGFX library itself is not included in the project. I tried all available code generators, but none of them added the library.