STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1565 Views
  • 0 replies
  • 2 kudos

Resolved! How can I set Interrupt priority with STM32CubeMX 6.0.1?

If I natigate to "Pinout & Configuration > System Core > NVIC" I get a table of interrupts. This table shows those which have been enabled, their preemption priority and subpriority. Some of the priority entries have a note "Managed by RTOS". Yes I a...

Mike xx by Associate III
  • 3830 Views
  • 1 replies
  • 1 kudos

I'm using S32cubeMX to create a project for a stm32L010; on a proprietary board we connected a SPI ST mems to USART2. I have 2 questions 1) I can't select MSBFIRST bit using standard HAL drivers. 2) it seems USART2 tx/rx lines have an internal shortcut

1) CubeMX create a usart type port, without opportunity to use UART_AdvFeatureConfig(); I implemented by myself the setting of MSBFIRST bit and works fine.2) using USART2 in synchronous mode, on the read operation tx and rx lines are exactly equal a...

Makefile toolchain corrupts makefile

A blank project with the Makefile toolchain will cause the following issue# C includes C_INCLUDES = \ -ICore/Inc \ -IDrivers/STM32F4xx_HAL_Driver/Inc \ -IDrivers/STM32F4xx_HAL_Driver/Inc/Legacy \ -IDrivers/CMSIS/Device/ST/STM32F4xx/Include \ -IDrive...

William1 by Associate II
  • 1333 Views
  • 1 replies
  • 0 kudos