STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1276 Views
  • 0 replies
  • 2 kudos

CubeMX doesn't allow Fadc > 18 MHz for H743 Rev. V

If from the "Clock Configuration" tab Fadc > 36Mhz then the Clock prescaler for the ADC is automatically set to /2 where the /1 is diabled. For > 72MHz it is /4 where /1 and /2 are disabled. Rev. 2 has an additional /2 divider that has been taken int...

Wde G.1 by Associate II
  • 1078 Views
  • 1 replies
  • 0 kudos

Resolved! if i will add any peripherals in existing code , existing code is disappear. new fresh code is generated

Hi, I am using STM32CUBEIDE, project creation is simple. i modified that code and i add the more function. After i need to add another peripherals, so i use .ioc (stm32cubemx) add another peripherials , after save it ask create, when into my proje...