STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1559 Views
  • 0 replies
  • 2 kudos

Resolved! LL_ Driver not part of IDE workspace. (F411RE)

When i open an example project everything works OK. When i create a project using CUBEMX or the IDE i see a limited number of drivers. Working with STM32F411RE. I don't see any LL Drivers.

PKAci.1 by Associate II
  • 1800 Views
  • 4 replies
  • 0 kudos

Resolved! "Required Ram or flash size for network is bigger than available Ram or Flash" alert with X-Cube_AI extension

Hi, I'm trying to load my Keras model (built for CamVid dataset) into STM tool, but when I try to analyze even with compression set to 8 it gives me the "Required Ram or flash size for network is bigger than available Ram or Flash" alert.I tried to m...

0693W000006EkSrQAK.png 0693W000006EkT1QAK.png 0693W000006EkT6QAK.png
LForm.1 by Associate II
  • 3823 Views
  • 7 replies
  • 0 kudos

Resolved! error: selected processor does not support `dsb 0xF' in Thumb mode

Hi,I am trying to generate code for STM32L010C6T6.using CubeMX5.5.0 & Atollic 9.0.1 IDE..After generating a code, I build it. I found errors likeselected processor does not support `cpsid i' in Thumb mode selected processor does not support `dsb 0xF'...

Bs.1 by Associate II
  • 2252 Views
  • 3 replies
  • 0 kudos