2020-04-20 5:18 AM
Hi,
I've recently started using STM32CubeMX and I tried installing newest Arm CMSIS 5.7.0, but whenever I do that I get the following error.
Errors:
- Ërror: Line= 633 : cvc-enumeration-valid: Value 'Cortex-M55' is not facet-valid with respect to enumeration '[SC000, SC300, Cortex-M0, Cortex-M0+, Cortex-M1, Cortex-M23, Cortex-M3, Cortex-M33, Cortex-M35P, Cortex-M4, Cortex-M7, ARMV8MBL, ARMV8MML, ARMV81MML, Cortex-R4, Cortex-R5, Cortex-R7, Cortex-R8, Cortex-A5, Cortex-A7, Cortex-A8, Cortex-A9, Cortex-A15, Cortex-A17, Cortex-A53, Cortex-A57, Cortex-A72, Cortex-A73, other]'. It must be a value from the enumeration.
- Ërror: Line= 633 : cvc-attribute.3: The value 'Cortex-M55' of attribute 'Dcore' on element 'processor' is not valid with respect to its type, 'DcoreEnum'.
- Ërror: Line= 1037 : cvc-enumeration-valid: Value 'Cortex-M55' is not facet-valid with respect to enumeration '[SC000, SC300, Cortex-M0, Cortex-M0+, Cortex-M1, Cortex-M23, Cortex-M3, Cortex-M33, Cortex-M35P, Cortex-M4, Cortex-M7, ARMV8MBL, ARMV8MML, ARMV81MML, Cortex-R4, Cortex-R5, Cortex-R7, Cortex-R8, Cortex-A5, Cortex-A7, Cortex-A8, Cortex-A9, Cortex-A15, Cortex-A17, Cortex-A53, Cortex-A57, Cortex-A72, Cortex-A73, other]'. It must be a value from the enumeration.
- Ërror: Line= 1037 : cvc-attribute.3: The value 'Cortex-M55' of attribute 'Dcore' on element 'accept' is not valid with respect to its type, 'DcoreEnum'.
- Ërror: Line= 1185 : cvc-enumeration-valid: Value 'Cortex-M55' is not facet-valid with respect to enumeration '[SC000, SC300, Cortex-M0, Cortex-M0+, Cortex-M1, Cortex-M23, Cortex-M3, Cortex-M33, Cortex-M35P, Cortex-M4, Cortex-M7, ARMV8MBL, ARMV8MML, ARMV81MML, Cortex-R4, Cortex-R5, Cortex-R7, Cortex-R8, Cortex-A5, Cortex-A7, Cortex-A8, Cortex-A9, Cortex-A15, Cortex-A17, Cortex-A53, Cortex-A57, Cortex-A72, Cortex-A73, other]'. It must be a value from the enumeration.
- Ërror: Line= 1185 : cvc-attribute.3: The value 'Cortex-M55' of attribute 'Dcore' on element 'require' is not valid with respect to its type, 'DcoreEnum'.
- Ërror: Line= 1189 : cvc-enumeration-valid: Value 'Cortex-M55' is not facet-valid with respect to enumeration '[SC000, SC300, Cortex-M0, Cortex-M0+, Cortex-M1, Cortex-M23, Cortex-M3, Cortex-M33, Cortex-M35P, Cortex-M4, Cortex-M7, ARMV8MBL, ARMV8MML, ARMV81MML, Cortex-R4, Cortex-R5, Cortex-R7, Cortex-R8, Cortex-A5, Cortex-A7, Cortex-A8, Cortex-A9, Cortex-A15, Cortex-A17, Cortex-A53, Cortex-A57, Cortex-A72, Cortex-A73, other]'. It must be a value from the enumeration.
- Ërror: Line= 1189 : cvc-attribute.3: The value 'Cortex-M55' of attribute 'Dcore' on element 'accept' is not valid with respect to its type, 'DcoreEnum'.
- Ërror: Line= 1190 : cvc-enumeration-valid: Value 'Cortex-M55' is not facet-valid with respect to enumeration '[SC000, SC300, Cortex-M0, Cortex-M0+, Cortex-M1, Cortex-M23, Cortex-M3, Cortex-M33, Cortex-M35P, Cortex-M4, Cortex-M7, ARMV8MBL, ARMV8MML, ARMV81MML, Cortex-R4, Cortex-R5, Cortex-R7, Cortex-R8, Cortex-A5, Cortex-A7, Cortex-A8, Cortex-A9, Cortex-A15, Cortex-A17, Cortex-A53, Cortex-A57, Cortex-A72, Cortex-A73, other]'. It must be a value from the enumeration.Obviously there is a problem since CMSIS schema changed to 1.6.3, whereas Schema 1.6.2 which this gets validated against doesn't contain eg. Cortex-M55. CMSIS 5.6.0 installs fine.
Is there any way that I can change the file that is used for this validation?
This is happening on MacOS 10.15.4 with STMCubeMX 5.6.1. I tried looking for the right file inside the app folder and in my ~/.stmcubemx and ~/.stcufinder but couldn't find the right file.
Thank you in advance.
2020-04-20 8:48 AM
Hello @kj.obara
Thanks for the feedback, issue detected.
It will be fixed next STM32CubeMX version.
Best regards,
Nesrine
2020-05-01 11:31 AM
I am also getting same error still when i try to install CMSIS with either STM32CubeMX or STM32CubeIDE.
When will be the next version release? Please comment
2020-05-01 11:58 AM
Is there way to work around with this issue?
2020-05-07 7:19 AM
I'm facing the same issue, when will it be fixed? can you please give us an idea?
Thanks,
Andrea
2020-05-31 1:05 PM
Same issue here.
2020-05-31 1:37 PM
Hello,
Issue reported to the tool development team that will plan the correction.
Best regards,
Nesrine