User Activity

I see G4 as successor of L4 for demanding applications, but I noticed DFSDM that is available on many L4s is not available on G4. Out of curiosity: is there a reason for it? Is there a replacement technique I might not be aware of?thanks!
Apart from the V_RMS, I_RMS, power and energy (all aggregated), is it possible to output the ADC readings real time over SPI? I am looking to get 8k samples of I and V out of it. As of it was a pure ADC, with the filtering, but without the calculatio...
I thought I ran into a bug when CubeMX could not configure oversampling for an F767 after I had used it on the less powerful L4. Read the reference manual and understand it is not there. Could not find which non-L families DO have oversampling. Hence...
Setting the RTC from the network time. Connecting to www.gandi.net at ipaddress: 151.101.37.103 200241d8 => C:\STM32CubeExpansion_Cloud_AWS_V1.4.0\Middlewares\Third_Party\mbedTLS\library\ssl_tls.c:4643: x509_verify_cert() returned -9984 (-0x2700)   C...
Kudos from