STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1628 Views
  • 0 replies
  • 2 kudos

Problem with packages in STM32Cube

Hello, I can't download none of packages in STM32CubeMX. There is error with message ".... not available...".  Trying to install manually causes error message "...Problem During Unzip File....". Trying to set the path to Firmware location manually in...

IBely.3 by Associate II
  • 4787 Views
  • 8 replies
  • 0 kudos

Resolved! STM32CubeMX STM32H750 I2S2 pin configuration.

I want to use the STM32H750. I want to configure the I2S2 to use the port PI0..PI1, but the CubeMX tool will not alloud me to do it. According the data-sheet it should be posible.Br. Poul-Erik.

Poul-Erik by Associate II
  • 1852 Views
  • 2 replies
  • 1 kudos

Resolved! NUCLEO-H743ZI USB printf works in STM32CubeIDE but not in Keil

I have a problem with using the printf function in Keil. I used the STM32CubeMX to setup a project and generated the code for Keil. All settings in CubeMX is standard, only thing changed is the USB_DEVICE set to Communication Device Class (Virtual Po...

LKris.1 by Associate II
  • 2550 Views
  • 3 replies
  • 0 kudos

GPIO User Labels not generated for dual core STM32H745ZIT

I use the last release of STM32CubeIDE (v1.1). When User Labels are defined for such peripherals as UARTs, TIMERs,..., defines are well created in main.hBut, when I define User Labels for simple GPIOs (inputs or outputs), nothing is generated in main...

M_Deloizy by Associate II
  • 1834 Views
  • 2 replies
  • 2 kudos

Resolved! STM32H7, STM32F7 cache enabled and MPU disabled

I'm using STM32H723, and STM32F767. CubeMX allows the data cache to be enabed and leave MPU disabled. Is this a valid configuration? Yes, i do know how to configure the MPU. Am i required to enable the MPU and configure all regions to have same attri...

BVu by Associate III
  • 3194 Views
  • 1 replies
  • 0 kudos

Resolved! TickPriority not assigned to uwTickPrio

Hello,Issue 1: assert_failed() triggeredI had observed an issue wherein the file stm32h7xx_hal_timebase_tim.c generated by STM32CubeMX for STM32H753BIT6 has HAL_InitTick() implementation different from what is provided on the GitHub repository of STM...

Resolved! STM32L4 with FreeRTOS and eMMC FATFS

Hi, I have custom HW with STM32L496RGTx. On board I have MicroSD card slot.I would like trying emmc from Hardkernel with microSD reader like this: I use CubeMX 6.1.1 with STM32L4 v1.16.0 package. If I set sdmmc1 to MMC 1bit in FATFS doesn`t offer SD ...

0693W000006HL21QAG.jpg 0693W000006HL2aQAG.png
lorant124 by Associate III
  • 3806 Views
  • 5 replies
  • 0 kudos