STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1572 Views
  • 0 replies
  • 2 kudos

Adding Keil MDK built library to the Cube project

I have a Keil MDK project which outputs a library mc_comms.lib. I have another Keil project which uses this library and there are any issues. My customer is using STM Cube and can't build the same test project with the same library. Here are the erro...

baruch by Associate II
  • 3603 Views
  • 7 replies
  • 0 kudos

variable assign error while using HyperBus OSPI RAM on L4R5

osram_init(3,1,2,6); // Initialized with Prescaler=3, HighSelect=1, tRWR=2,tACC=6, MemoryMap, refer to CUBE-MX L4R9Eval OSPI_MemoryMap example Project uint8_t* mem_addr = ( uint8_t * )( OCTOSPI1_BASE + 0 );   *mem_addr = 0xF0;   *(mem_addr+1) = 0x...

Lee.Lys by Associate
  • 708 Views
  • 0 replies
  • 0 kudos

STM32CubeMX does not copy custom_motion_sensors.c and custom_motion_sensors_ex.c files when the code is created.

STM32CubeMX does not copy custom_motion_sensors.c and custom_motion_sensors_ex.c files when the code is created. Has anyone come across this issue, if yes what was the issue? I have checked in and out but unable to find the issue. I have checked the ...

0693W000008xL7XQAU.png
Shaun.t by Associate III
  • 758 Views
  • 0 replies
  • 0 kudos

Resolved! SMBus STM32F439 HAL Driver

Hi all,I read STM32F4 MCU family doesn't support SMBus because of hardware limitations in the I2C cell. For this reason SMBus is not included in the HAL driver. If I choose STM32F439ZI in STM32CubeMX and I activate I2C, I can select between 3 differe...

0693W000008x25NQAQ.jpg
AFara.2 by Associate II
  • 2858 Views
  • 2 replies
  • 0 kudos