cancel
Showing results for 
Search instead for 
Did you mean: 

Can't get ADC DMA to work with STM32H743

EMarq.1
Associate II

I'm using a 32H743 with CubeMx and Keil. I want to do DMA on a single ADC channel. In Cube I set up the ADC in Continuous Conversion Mode, Regular Conversion launched by software, and set the Conversion Data Management to DMA Circular Mode., and set DMA1 Stream 0 in circular mode. In Keil, I set up the buffer and call HAL_ADC_Start_DMA and also have the HAL_ADC_ConvHalfCpltCallback and HAL_ADC_ConvCpltCallback functions added. However, neither callback is reached. It appears the ADC works at least once as I get a correct value in the ADC data register. However, the DMA1 S0CR register doesn't have the EN bit set for some reason. If I force it on manually it gets reset somewhere in HAL_ADC_Start_DMA.

I can do this first time using the STM32F413 so I think my basic procedure is correct, there's some difference between the F413 and H743 that's messing me up. Any ideas?

Thanks

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
TDK
Super User

Sounds like DMA might not be fast enough to keep up, in which case the DMA stream will disable itself and raise an error status flag.

If you feel a post has answered your question, please click "Accept as Solution".
EMarq.1
Associate II

I don't think that's it - I see the same problem on the H743 even if I increase the sampling time to the maximum (810.5 cycles, and I was already running at just 4 MHz clock). No problem with the F413 at 3 cycle sample time and 16 MHz with divide by two. Also, HAL_ADC_Start_DMA, which is where the enable disappears, returns 0 so no sign of an error.