STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1626 Views
  • 0 replies
  • 2 kudos

Why in CubeMX the sum of the two parameters must be be 32?

New question split from this thread. Hello, Thank you for your response. I have double-checked and found that the 6.10 version also cannot be configured in this way. I will adopt the single-line mode on the next hardware version. However, there is s...

BJX_0-1764905583381.png
BJX by Associate II
  • 567 Views
  • 1 replies
  • 1 kudos

Resolved! Cube MX - Product Search Filters

Hi, I'm trying to understand what filters I have to apply in CubeMX to find products that support 2 QUADSPI with independent clock. E.g. h7a3aii6q seems to be such part that allows me to have two independent  QUADSPI and there are parts like e.g. H74...

b3rtl by Associate II
  • 285 Views
  • 1 replies
  • 0 kudos

Resolved! Linker Errors when enabling CMSIS RTOS v2 and TrustZone

I have started a new project using STM32H573. This is using the following:Cube MX 6.16Cube IDE 2.0 - Build: 26820_20251114_1348 (UTC)The project has secure zone enabled. I have written bare metal code and shown I can run/debug code in the non-secure ...

NickO by Associate III
  • 1081 Views
  • 7 replies
  • 0 kudos

Resolved! STM32U073 SWO Debug not available?

So here is a weird thing I've noticed with a STM32U073... CubeMX shows that this CPU has the "Trace Asynchronous SW" option, but for this mcu it is no longer listed under SYS, but under its own category: "Trace and Debug" -> "DEBUG". Anyway, after en...

S13 by Associate II
  • 1225 Views
  • 7 replies
  • 4 kudos