User Activity

Hi,I am using the latest version v1.16.0 STM32CubeIDE with stm32g071cb.It is not possible to use ADC1_IN16 (PB12). I have created also a new project  to test this condition.Changing the sequencer disables IN16 or makes error condition.I need PA2 -PA3...
It is same error for me with stm32g071cbt6 I just made a new project. And tried to use ADC1_IN16 pin for analog conversion. Still I can not use ADC1_IN16 Do you have a solution?
I have 2 different projects, different folders, different *.ioc files (project1 and project2)But one of them is related to other one.When I open the project1, the project2 is opens automatically.After that when I closed the project1, the project2 can...
Hi,I am using Stm32CubeIDE v1.3.1 with my custom STM32F746IG board and touchGFX enabled (working properly with 800x480 paralel LCD). I have tried to play with DAC channels (Channel1-2). I can not get it work through the examples with DMA enabled or w...
After installing the cubeProgrammer, Dfuse software is not recognizing the STM devices. STM32Cube programmer is OK. But we have customers that uses Dfuse and already documentated how to update devices via Dfuse. Is it possible to work properly again ...
Kudos from
Kudos given to