STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1572 Views
  • 0 replies
  • 2 kudos

Resolved! CubeIDE, STM32F446RE and SAI2

As datasheet states (more than once) the LQFP64 package of the 446RE has 2 SAI blocks (both with SAI-A and SAI-B) and in the HAL driver/definitions stm32f446xx.h both are available, but I'm not able to select the 2nd SAI in Cube (it is not shown ther...

ACAV by Associate II
  • 2678 Views
  • 4 replies
  • 1 kudos

software packs question about STM32L5

Hi,I can add "X-CUBE-AZRTOS-L5_V1.0.0_M33NS" via "Pinout & Configuration->Software packs->Select Components" successfully, but failed at add "X-CUBE-AZRTOS-L5_V1.0.0_M33S".Please check the attachment.Your example "Tx_SecureLEDToggle_TrustZone.ioc " ...

zqizh.1 by Associate III
  • 1767 Views
  • 1 replies
  • 0 kudos

CubeIDE : support for more than one cubeMx project

I actually have a Nucleo and a custom board. They are running same software and are very identical in terms of hardware but not identical: but there is at 2 pins that need to be changed and UART added: set baud rate, set NVIC IT. I also have to inser...

DaDude by Associate II
  • 1662 Views
  • 3 replies
  • 0 kudos

Resolved! STM32CubeIDE creates main.c but I am using main.cpp!

I converted project from C to C++ with right click on project-> Convert to C++. The problem occurs when I generate the code in graphic configurator . It creates main.c file. Which is also loaded to controller if I run it. How to solve this problem?

0693W00000GZecYQAT.png
MAnto.2 by Associate III
  • 4473 Views
  • 3 replies
  • 2 kudos

using variables / constants in .ioc file from main?

Good afternoon....Can someone tell me how to use constants that are #defined in main back in the .ioc file? I have run the CubeMX and generated the ioc file then generated main. I then do work in main and make some changes to the initialization fea...

SWenn.1 by Senior III
  • 2701 Views
  • 6 replies
  • 0 kudos

Getting GPIO pin to toggle in Blinky

I'm trying to get my embedded skills back from many years ago, so I have an STM32L475 L475E board I am working with. I am using Blinky to reference from, but I can't get the output pin to toggle in the thread for the flashing led./* Private defines -...

BEppe.1 by Associate II
  • 4231 Views
  • 5 replies
  • 0 kudos