STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1688 Views
  • 0 replies
  • 2 kudos

I2C timing setup for STM32L552MEYxP

Hello all,  I have a STM32L552MEY6P. I am using it as a slave and setting an address. Using the MX cube set the speed for 400kHz. I have a Rasberry pi trying to do an address detect. Whenever I turn on the clock stretch, I get a read at address 0x50....

0693W00000LzWINQA3.png 0693W00000LzWIXQA3.png
VThan.2 by Associate III
  • 1157 Views
  • 1 replies
  • 0 kudos

If I activate the LSE for the RTC instead of the LCI, using version 6.4 of stm32cubemx , the "SystemClock_Config()" function generates an error. is there a solution to solve the problem using version 6.4 of stm32cubemx.

Initially I used version 6.5 of stm32cubemx to generate my project for stm32h743 and as I use the ADC module which I cannot get to work with this version, I switched to version 6.4, I So the problem of the ADC is solved, it works very well except tha...

Resolved! STM32CubeIDE modify HAL code

We have to make minimal changes to parts of the HAL code, which would be overwritten by code generation.Is there a recommended way to implement such changes, such that they don't get reverted by generation?The two ways I can think of both have their ...

JKut by Associate II
  • 1447 Views
  • 1 replies
  • 0 kudos

Why don't I have HAL_CAN_Transmit in the generated CubeMX code?

I setup a project in CubeMX (STM32F302C6), activated CAN (and other peripherals) and did everything. I generated the code and opened it in eclipse. However, in the HAL_CAN library the functions like HAL_CAN_Transmit are missing. I have these control ...

YFric by Associate II
  • 5872 Views
  • 6 replies
  • 0 kudos

Resolved! How to set DIVN2 and DIVP2 of PLL2 in code

I have set the clock for the ADC to 51.2MHz by PLL2P with the DIV set as seen below. Without reprogramming the STM32H7A3 I would like to change DIVN2 to x16 and DIVP2 to /32 to give me 4MHz clock to the ADC, but I can not seem to find where these are...

0693W00000NqiT8QAJ.png
KSOdin2 by Associate III
  • 4403 Views
  • 11 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.