User Activity

Hi,I am using a custom board with stm32H473 to driving a GUI on 9 inch RGB TFT screen.I have 10 screen which when I switch between them and main screen, some times TouchGFX hangs on this state, but other threads and debugger work fine, The only diffe...
Hi,I've used STM32CubeMX to configure my STM32H7 MCU, but RTC initial values which I set on CubeMX as default value are not set on RTC_TR and RTC_DR registers after debugging line by line when  MX_RTC_Init() is called. There is no fault reported or a...
Hello, I have problem with touchGFX once i updated it from 4.16.1 to 4.17 .... when touchgfx_init() function reached to this line (FrontendHeap& heap = FrontendHeap::getInstance();) it makes hardfault which i have not on previous version....in assemb...
Hello,I worked with TouchGFX 4.16.1 fine, because of graph issue in 4.16, i've migrated to TouchGFX 4.17 and also CubeMX 6.3 ... after this updating touchgfx_init() function produce hardfault .... Please help me how can I solve this issue ....I work...
Hi, I Have a custom board with stm32h743... I design a graph page with touchGFX and when D-cache is enable, system detect some hard faults specifically when I touch a button to change screens, some times it works and some times not, When I disable D-...
Kudos from