STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1584 Views
  • 0 replies
  • 2 kudos

Running into Secure Fault on STM32U5 after Timer starts

I am using the example project GPIO_IOToggle_TrustZone for NUCLEO-U575ZI-Q and added Timer3 for Non-secure application via CubeMx with Interrupts enabled. When this Timer is started with HAL_TIM_Base_Start_IT the application runs into SecureFault_Han...

LBöhm.1 by Associate III
  • 1162 Views
  • 1 replies
  • 0 kudos

NVIC_SetVectorTable() API not available in HAL

Hello There,I'm working on IAP app and need to relocate vector table and came across NVIC_SetVectorTable().But I'm not able to find this API. I'm using CubeIDE and did generate the initial code with inbuilt cube mx. Any help is appreciated.Regards,Ke...

KAgga.1 by Associate III
  • 3203 Views
  • 4 replies
  • 0 kudos

How to add a CubeMX configuration file to Simulink?

I am currently working on a project that would require me to access a STM32 microcontroller from Simulink. I am going to be using the STM32L476RG momentarily and STM32F722ZE in the future. I have tried using the STM32-Mat file, but it doesn't allow m...

MArvi.1 by Associate II
  • 1045 Views
  • 0 replies
  • 0 kudos

Need help to read Accelerometer with I2C DMA

I'm try to read acceleration from KX132 accelerometer with a STM32F446ZE through I2C with DMA. I create a project with STMCubeMX and enable DMA and interruptions.The accelerometer has six register each one of 1 byte where save acceleration in this fo...

polgu.1 by Associate II
  • 1597 Views
  • 1 replies
  • 1 kudos