STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1560 Views
  • 0 replies
  • 2 kudos

How to setup gitlab ci for STM32CubeMX?

Hi guys,I am very new to continuous integration. My company has tasked me to set up a gitlab ci for there STM32CubeMX project. They want the following:A self hosted gitlab on a docker container on a machine (This I have already set up)Gitlab runner o...

Tamper button does not work on cm4

I am using an STM32H757-eval board. From the CM7 I can detect a Tamper button press (PC13). I would like to detect this same button press from the CM4. Using CubeMX, I assign PC13 to the CM4. After rebuilding, I am not able to detect Tamper button pr...

Gil1 by Associate III
  • 3547 Views
  • 8 replies
  • 0 kudos

Multiple adc conversions using DMA (help please)

1.volatile uint16_t ADC_Value[4];-this is my array for the values to be stored2.void ADC1_Configure(void) {  ADC_InitTypeDef ADC_InitStructure;     ADC_InitStructure.ADC_Mode = ADC_Mode_Independent;  ADC_InitStructure.ADC_ScanConvMode = ENABLE;  ADC_...

hpark.21 by Associate
  • 1405 Views
  • 2 replies
  • 0 kudos

FreeRTOS code generation bug on V6.7.0

Hello,After creating a blinky project in CubeIDE version 1.11.0 running on Linux and setting up FreeRTOS within the .ioc file, the default task fails to run.A project created with STM32CubeMX V6.6.1 works, but when it was migrated to V6.7.0 (by openi...

NWrig.2 by Associate
  • 1873 Views
  • 2 replies
  • 0 kudos