STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1555 Views
  • 0 replies
  • 2 kudos

Resolved! STM32CubeMX I2C on STM32H563

Hi,I use STM32CubeMx 6.9.1 on a STM32H563 project. Programming the I2C pins, there is no way to setup the I2C_SCL pin as Alternate PushPull. Only the Alternate Open Drain is possible. Why?In my application, the I2C_SCL pin is connected to a serial EE...

Ez by Associate II
  • 3259 Views
  • 4 replies
  • 0 kudos

inference array input and serial monitor

I'm trying to run inference of Onnx model. I tried to use the manual 'How to run locally a c-model'. in all the guides I found the input for the network is one number in my case the input is array of[1][32][101].I want to inference the array once so ...

audi by Associate II
  • 1127 Views
  • 0 replies
  • 0 kudos

Resolved! IMPOSSIBLE UPDATE STM32CUMEMX

Hello everyone. I installed STM32CUBEMX and STM32CUBEIDE on my Windows 11 and use them so as to get updates from STM32CUBEIDE but I can not update STM32CUBEMX : on the home page of CUBEMX when I click on "CHECK UPDATES" opens the window "Check Update...

rdl by Associate III
  • 3522 Views
  • 2 replies
  • 0 kudos

Resolved! Will STM32CubeMX support FreeRTOS for STM32U5-series?

Hi there,I would appreciate support in CubeMX for FreeRTOS for STM32U5-series. Currently I cannot find out how to configure this via the tool.FreeRTOS.org recently released a demo for IoT Reference Integration, running on an STM32U5. My old code is w...

KHofm.1 by Associate II
  • 4613 Views
  • 5 replies
  • 1 kudos

Resolved! Issue in "STM32 MCU product selector" and CumeMX

I'm looking for M7 core in UFBGA169 Package with 3 ADC units.According to "Analog" part of table devices like H747AI, H753AI, H757AI have no ADC!The same problem exists in Cube Target selector: when I move "ADC Total (converters) to "1" or more, the...

DrDro by Associate III
  • 1915 Views
  • 4 replies
  • 1 kudos

Resolved! I2C error codes F767ZI

I am working to get one F767ZI board (master) to send 1 byte to a second F767ZI (slave).  I'm using 4k external pull-up resistors on SDA and SCL.  I am trapping errors in the master and they are:After the following code on the master I get "Error 32"...

RPatt.11 by Associate II
  • 4502 Views
  • 5 replies
  • 3 kudos

Resolved! Purpose of HAL_FLASH_Program_IT from CubeMX on NUCLEO-F746ZG?

Hi,I was wondering what is the purpose of the API HAL_FLASH_Program_IT(..) provided by CubeMX (based on NUCLEO-F746ZG but seems to be widely the same for other MCU references..).As it allows to write a single value at a time it seems useless to attem...

Nadreoh by Associate III
  • 2896 Views
  • 3 replies
  • 1 kudos

How to access spdifrx_symb_ck

In the reference manual: https://www.st.com/resource/en/reference_manual/rm0468-stm32h723733-stm32h725735-and-stm32h730-value-line-advanced-armbased-32bit-mcus-stmicroelectronics.pdf there is a clock symbol mentioned called: spdifrx_symb_ck which is ...

etheory by Senior II
  • 3659 Views
  • 8 replies
  • 1 kudos