STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1578 Views
  • 0 replies
  • 2 kudos

cubemx 6.3.0,STM32L562VETx,sd+FATFS,BSP code for SD

    Nothing generated by CubeMx: the BSP code has to be added to the project according to the board (ST or custom) in use.   ​Does this MCU need to manually transplant the BSP of SD card?Why did the F103 and f429 MCU have the corresponding BSP code f...

0693W00000D1iYIQAZ.jpg 0693W00000D1iXEQAZ.jpg
MShao.1 by Associate III
  • 2095 Views
  • 2 replies
  • 2 kudos

Can not execute f_open

I have connected microsd by SDIo to STM4Disc1 board. I am using SD 4 bit.  I see on STM forums there is a bug and needs to set 1bit in MX_SDIO_SD_Initso I changed to   hsd.Init.BusWide = SDIO_BUS_WIDE_1B and reduce SDIO CLK by 192 factor.I am able to...

Nico3 by Senior
  • 1763 Views
  • 3 replies
  • 0 kudos

Problem with IDE

Hello, I've got problem with STMCubeIDE. You can see my problem at photos I attached. Can anyone help me to solve this problem. I try to work on Lenovo Legion 5 with Ryzen 5 5600h and RTX3060. Second graphic card is integrated with Ryzen CPU. This pr...

Resolved! CubeMX ioc-File corrupt

Dear Sir and Madam,I started a new project with STM32H745 from scratch. After implementation of all pin function and names, I worked on the clock tree. During this, I saw, one UART must be changed to the FDCAN interface. While doing this, CubeMX was ...

JPiet.3 by Associate III
  • 5828 Views
  • 4 replies
  • 0 kudos

issue after migrating to new version STM CUBE MX

Hi everybody I have errors in code mainly in RTOS file and TASK file after Updating the new STM32 CUBE MX generating code any one have any idea about these things  note :My code is working fine with old version of STM cube Mx i am using IAR workbench...

PESHWA by Associate II
  • 1195 Views
  • 1 replies
  • 0 kudos