STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1547 Views
  • 0 replies
  • 2 kudos

Resolved! STM32CubeIDE while(1) bug? Linux versions

Hello, I see in code generated by all Linux versions of CubeIDE that USER CODE BEGIN and USER CODE END tags in infinite loop, are not in the better place.Code generated by Cude IDE: /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { ...

xisco by Senior
  • 1854 Views
  • 3 replies
  • 3 kudos

Resolved! SMPS Configuration

Using STM32CubeMX Version 6.11.1 for code generation of STM32U545RETxQ LQFP64.When pressing "Generate Code" there is a message recommending SMPS setting from the PWR menu.However, no SMPS there and not anywhere in the configuration menu. (Attached)An...

IP.2 by Associate II
  • 1690 Views
  • 1 replies
  • 0 kudos

Resolved! Fail to find a clock

Hello there,I’m trying to squeeze functionality into an STM32U5 MCU via the STM32CubeMX tool.After setting the pins, the clock configuration fails to find a solution.The requirements for the clock are to run from an internal source, as the design is ...

IP.2 by Associate II
  • 1323 Views
  • 2 replies
  • 0 kudos

Resolved! Does CubeMX's .exe file include virus?

Hi,I did setup CubeMX latest(6.13) and previous version , Kaspersky have seen virus and I ignored it. After that I got some malfunction on my pc like internet connection disabled, windows bar doesnt work. 

Zek_De by Senior
  • 3076 Views
  • 8 replies
  • 3 kudos

Resolved! STM32CubeMX/Simulink Compatability

Good Morning, I'm using Simulink to develop code for the STM32F767 MCU, however we're looking at moving to a newer micro (STM32H7R318T6). This MCU doesn't seem to be available in STM32CubeMX V6.4.0, which is the officially supported version, so I hav...

Resolved! FLASH.ld syntax error when upgrading to CubeMX v6.12.1

Hello,Since the latest release of CubeMX (6.12.1), I have been encountering syntax errors related to the "FLASH.ld" file. This issue only arises when I generate code while setting the Toolchain/IDE to CMake. I am using STM32H753IIKx. It seems that Cu...

OmidES by Associate II
  • 37712 Views
  • 45 replies
  • 57 kudos