STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1568 Views
  • 0 replies
  • 2 kudos

Resolved! SDIO and I2S MCLK output warning

I'm using a STM32F407VG (actually a disc-1 board). I've set I2S2 in full-duplex master mode and generating the MCLK out on PC6 for an external slave codec. So far so good.Now i want to set SDIO interface in full-duplex 4-bits mode but CubeMX throws a...

omaroski by Associate II
  • 210 Views
  • 2 replies
  • 1 kudos

Resolved! unknown type name 'size_t motion_fx.h

I created a motion_fx for stm32h562 from CubeMx. The auto generated motion_fx.h file does call (line 135)size_t MotionFX_GetStateSize(void);​But the code does miss the include #include <stddef.h>Which results in the following error:unknown type name ...

Resolved! HRTIM configuration when updated to 6.16.1 CubeMX

Hi,In STM32CubeIDE/MX versions 1.19 and 6.15, I configured HRTIM, and it worked fine without any errors in CubeMX. I have updated STM32CubeIDE/MX to versions 2.1.1 and 6.16.1, and I have noticed the error messages shown in the pictures below.The dead...

Pic1.jpg Pic2.jpg
kkolek by Associate
  • 288 Views
  • 1 replies
  • 0 kudos

How to use the USER_PHY

In a recent release (not sure which one) the option to select USER_PHY was added to the platform settings under LWIP.I need to implement a different PHY for a LAN9374. It is basically identical to the LAN8742. The only issue is that the LAN8742 init ...

theRat_0-1754960624856.png
theRat by Associate II
  • 1227 Views
  • 7 replies
  • 1 kudos

Resolved! Missing file after file generation

 Hello,I am encountering an issue with the ST example projects "BLE_p2pServer" and "BLE_DataThroughput_Server" for the NUCLEO-WBA65RI board.After generating the code using STM32CubeMX (version 6.17), the project does not include all the required sour...

Resolved! [BLE] CubeMX remove function in "custom_app.c"

Hi,I found an issue when generating code for a BLE application with STM32CubeMX v6.17.0.In particular, I have a service called DataTransferService with three characteristics:DataStreamCommandControlTransferStatusThe DataStream characteristic is confi...