Skip to main content
MMeie.3
Associate II
April 10, 2025
Solved

STM32H562 SRAMx_ECC wrong description in CubeMX

  • April 10, 2025
  • 3 replies
  • 1579 views

Hi

We work on a project with a STM32H562. We use STM32CubeMX Version 6.14 with the Firmware Package V1.5.0 to generate a STM32CubeIDE project on Windows 11. I just found a wrong description in CubeMX.

The description for SRAM2_ECC, SRAM3_ECC and BKPRAM_ECC, says the parameter in CubeMX needs to be set to “Disabled” to enable ECC check.

Assuming I want to disable ECC, I would set the option to “enable” in CubeMX. CubeMX then adds OB_SRAM2_ECC_ENABLE, OB_SRAM3_ECC_ENABLE and OB_BKPRAM_ECC_ENABLE in MX_FLASH_Init(). All three options are defined in stm32h5xx_hal_falsh_ex.h as 0. According to chapter 7.11.24 of the reference manual, setting the bit to 0 in the register, enables ECC (exactly the opposite of what I wanted). Therefore, the description in CubeMX is wrong. To Disable ECC, configure Disable in CubeMX and to enable ECC, configure enable.

MMeie3_1-1744271578960.png

 

MMeie3_0-1744271548478.png

 

This topic has been closed for replies.
Best answer by MMeie.3

@Ghofrane GSOURI I just tried the new STM32CubeMX 6.15., and at least in my current project the issue is fixed.

3 replies

Ghofrane GSOURI
ST Technical Moderator
April 10, 2025

Hello @MMeie.3 

First let me thank you posting.

I'm currently investigating this . I will get back to you asap.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Ghofrane GSOURI
ST Technical Moderator
April 10, 2025

Hello @MMeie.3 

Your detailed explanation is much appreciated.

Issue has been raised to he development team for fix.

Internal ticket number 207331

THX

Ghofrane

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
MMeie.3
MMeie.3AuthorBest answer
Associate II
July 8, 2025

@Ghofrane GSOURI I just tried the new STM32CubeMX 6.15., and at least in my current project the issue is fixed.