STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1591 Views
  • 0 replies
  • 2 kudos

Resolved! I2C speed problems

Hi everyone,I’m currently working on an I2C communication setup using the Nucleo-H753ZI DK but the cubeMx document is for the STM32H743BIT (the MCU for my custom board) and aiming to run it in Fast Mode (400 kHz). However, when configuring the I2C cl...

JonConesa_0-1741626901002.png JonConesa_1-1741627197068.png JonConesa_2-1741627277291.png JonConesa_3-1741627293171.png
JonConesa by Associate III
  • 7790 Views
  • 22 replies
  • 16 kudos

CUBEIDE Bug in RTC Generation

Hello,In CubeIDE I try to generate RTC code which has decimal parameters. However in code generation I realized that it converted to hex value by itself.You can check screen shots in the attachment. 

CubeMx MAJOR BUG in UsbX configuration....

I'm using ThreadX on a STM32H743 MCU.  I'm trying to setup a USB Host_only on the USB_HS device, and a USB Device_only device on USB_FS.  The peripheral configuration is okIn the AzRtos settings, it defines 2 seperate byte_pools for each device (one ...

mattcrc_0-1741644603541.png mattcrc_1-1741644669213.png mattcrc_2-1741644863409.png mattcrc_3-1741645010754.png
matt-crc by Senior III
  • 1329 Views
  • 1 replies
  • 0 kudos

Abnormal behaviour with STM32CubeMX

Hello, Hope you're well. I started a project with CubeMX to use makefiles. I am able to compile and flash to the board but the code does not run properly on the f4 discovery board. To debug, I used Keil on a windows system and the code is actually wo...

daded.1 by Associate II
  • 1319 Views
  • 2 replies
  • 0 kudos

LTDC Window Horizontal Stop and Vertical Stop: 800 or 799?

Hi,when configuring the LTDC for a 800 x 800 display, the Window Horizontal Start is by default set to 0 which suggests it is a 0-indexed range. So do you set the Window Horizontal Stop and Window Vertical Stop to 800 or to 799? As a separate questio...

Ricko_0-1741475158336.png
Ricko by Senior III
  • 1215 Views
  • 2 replies
  • 1 kudos

stm32u575 & Ethernet support On CubeMx

A new question moved from this thread to the correct forum board (to be answered by CubeMx team) Hi If STM32U5 has no support for Ethernet why in configurator i can enable the Middleware NetxDuo?  The question start from this point, NetxDuo support, ...

mauroalba by Associate II
  • 4774 Views
  • 1 replies
  • 0 kudos