cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX inconsistent indentation for MX_TouchGFX_Process()

 

If I enable USB host and TouchGFX without OS I get the following generated code:

  /* USER CODE BEGIN WHILE */
  while (1)
  {
    /* USER CODE END WHILE */
    MX_USB_HOST_Process();

  MX_TouchGFX_Process();
    /* USER CODE BEGIN 3 */
  }
  /* USER CODE END 3 */

As you can see MX_TouchGFX_Process() isn't indented properly.

I want this:

  /* USER CODE BEGIN WHILE */
  while (1)
  {
    /* USER CODE END WHILE */
    MX_USB_HOST_Process();
    MX_TouchGFX_Process();
    /* USER CODE BEGIN 3 */
  }
  /* USER CODE END 3 */

 

Kudo posts if you have the same problem and kudo replies if the solution works.
Click "Accept as Solution" if a reply solved your problem. If no solution was posted please answer with your own.
4 REPLIES 4
Souhaib MAZHOUD
ST Employee

Hello @unsigned_char_array 

Could you share the project or the name of the MCU that occur this issue ?

Thanks

Souhaib

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

STM32H735

Kudo posts if you have the same problem and kudo replies if the solution works.
Click "Accept as Solution" if a reply solved your problem. If no solution was posted please answer with your own.

I've attached an ioc file to reproduce the problem. I just created a fresh project for the STM32H735G-DK
with everything set to default and enabled TouchGFX and USB host.

Result:

 

  /* USER CODE BEGIN WHILE */
  while (1)
  {
    /* USER CODE END WHILE */
    MX_USB_HOST_Process();

  MX_TouchGFX_Process();
    /* USER CODE BEGIN 3 */
  }
  /* USER CODE END 3 */

 


Edit: still not fixed in STM32CubeMX V6.12.1

Kudo posts if you have the same problem and kudo replies if the solution works.
Click "Accept as Solution" if a reply solved your problem. If no solution was posted please answer with your own.

Still not fixed in STM32CubeMX V6.16.0

Kudo posts if you have the same problem and kudo replies if the solution works.
Click "Accept as Solution" if a reply solved your problem. If no solution was posted please answer with your own.