STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1626 Views
  • 0 replies
  • 2 kudos

STM32CubeMX together with KEIL mdk 5

Posted on September 30, 2016 at 11:08Hello, I have problems using STM32CubeMX together with KEIL mdk 5. When starting a new project in Keil I can use all the Keil functionality, but when I open Cube from the project runtime environment and initializ...

STM32CubeMX 4.14.0 bug report - gray comboboxes

Posted on March 26, 2016 at 23:44 I tried a new version 4.0 of STM32CubeMX. I selected the STM32F746G-DISCO board. If I set the Detect_SDIO GPIO: Input ad PC13, closed and openedthe ioc file, then the comboboxes are gray and you can not cha...

0690X00000604u2QAA.png

cubemx + errata

Posted on June 08, 2016 at 18:10I would propose to update the cubemx sw to consider also the errata/chip bugs, to implement the workaround (where there is one) or mark setting as invalid. The tool itself(cubemx) is a very good idea in general, it wo...

Full-Duplex I2S using STM32F7

Posted on October 04, 2016 at 12:48Hello, We want to use the Full-Duplex I2S interface in a STM32F7 (STM32F769NI) but the CubeMX only allow the Half-Duplex feature, and the libraries doesn't support it. Nevertheless, the STM32F4 Cube allows the Full...

Connect 2 board to each other with Ethernet Protocol

Posted on September 19, 2016 at 16:50hiI working with stmf429 board with cubemx and HAL driver and i must run ethernet protocol (with LWIP or without)I want to connect 2 boards to each other (for example press key and led light up in other board) I ...

hamrgh by Associate II
  • 1517 Views
  • 2 replies
  • 0 kudos

HAL CAN Bus Transmission Problem

Posted on September 08, 2016 at 16:57Hello,       I am trying to send 1000 values from data stored in DMA on to CAN Bus. i am using the Data frame(8 bits each) of CAN to transmit data but i am not able to receive all the data frames. i am not able t...

ninad911 by Associate III
  • 1785 Views
  • 2 replies
  • 0 kudos

STM32CubeMX FATFX + FreeRTOS

Posted on August 31, 2016 at 14:50Hello!I use STM32CubeMX, STM32F429ZIT microcontroller project contains FATFX and FreeRTOS. I have three questions:1) When the STM32CubeMXcode generates function MX_FATFS_Init () is in the code void StartDefaultTask ...

dr23 by Associate
  • 1105 Views
  • 2 replies
  • 0 kudos