STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1547 Views
  • 0 replies
  • 2 kudos

STM32CubeMX 4.22 SystemClock_Config Bug

Posted on September 07, 2017 at 21:43I am using STM32CubeMX 4.22.0I am using STM32F103C8T6 chip with Keil v5 under Windows 10.I configured only RCC to HSE  for Crystal\Ceramic Resonator and in Clock Configuration input frequency to 8 MHz and HCLK to...

HAL_RCC STM32L4 bug in definition

Posted on September 07, 2017 at 17:47Hi,I found a bug in the last version of stm32l4xx_hal_rcc.h from stm32L4 uC.file: stm32l4xx_hal_rcc.h/.cversion 1.7.2&sharpdefine __HAL_RCC_GPIOB_IS_CLK_ENABLED()it should refer to RCC_AHB2ENR_GPIOBEN instead of ...

possible cubemx or library bug?

Posted on July 14, 2016 at 01:05Hi,    I generated a project that included ADC2.  Multimode is set to independent.  When I run my project I get an error in MX_ADC2_Init.  When I trace it, the problem is in HAL_ADCEx_MultiModeConfigChannel().  At lin...

STM32CubeMX / C++ - Linkage Error in generated Code

Posted on June 26, 2017 at 11:49Hi,I want to use STM32CubeMX and I would like to program my new project in C++. I am using the latest version of STM32CubeMX (4.21.0) and the latest version of Keil uVision (5.32.0.0).After code generation I have adde...

smrtkai by Senior
  • 2608 Views
  • 3 replies
  • 0 kudos

I setup USB Host using STM32CubeMx. How can I receive data using USB Host and the USBH_CDC_Receive function and the CDC_ProcessReception(phost) ?

Posted on August 21, 2017 at 15:17I have setup the USB Host using the STM32CubeMx and I can transmit data in bulk and it has a state machine.  The USB is attached to the host which is a CDC USB Modem.  The CDC_ProcessReception(phost) does not receiv...

BUG CubeMX 4.20.1 and RTC

Posted on April 13, 2017 at 16:19hi to all, i use a  cubemx 4.20.1 for configure STM32L152RE; when i configure the RTC pin with alarm A  i see a error handler.indeed when the system arrived to LSE configuration i have a HAL_TIMEOUT, can you help me?...

antonioB by Associate II
  • 2304 Views
  • 5 replies
  • 0 kudos

STM32F407 + UDP+LWIP big packet problem

Posted on August 16, 2017 at 00:58Dear Forum,I bring forth a frustration question yet I'm uncertain how to approach it.I have STM32F402, and I can communication over UDP . In cube I reviewed every options but my problem do not solved. If I can sendi...

lorant124 by Associate III
  • 1348 Views
  • 1 replies
  • 0 kudos