STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1564 Views
  • 0 replies
  • 2 kudos

Why would anyone use STM32CubeMX if STMicro doesn't?

I have the STM32F769 Discovery kit to evaluate using the F7 for a future project. I want to enable a timer input, so rather than claw through the poorly written examples (for instance, the TouchGFX example doesn't even load onto the chip) I thought I...

MPlan.7 by Associate III
  • 6542 Views
  • 12 replies
  • 2 kudos

I can't get the ouputs to do anything.

I'm using STM32CubeMX and Atollic's TrueStudio to make a simple program that writes to the serial port and turns on and of ports B3 and B4.I've tried every possible combination in the GPIO section of Pinout & Confiuration of CubeMX and can't read any...

Dan in WY by Associate III
  • 4686 Views
  • 14 replies
  • 0 kudos

STM32CubeMX V5.1.0: error in ADC.

During the ADC configuration for STM32G071RB in CubeMX, the program hangs. This is only for ADC. I checked it on two computers.

wuio by Associate II
  • 3956 Views
  • 7 replies
  • 0 kudos

File corruption after eMMC formatting

Hi all,I am using cubeMx code base for interfacing eMMC with controller STM32L496QGI6. With the support of FAT FS, I could write/read files to/from eMMC. But I am having two issues.#issue 1. Getting issues after formatting emmc from the device( by us...

STM32CubeMX hangs at code generation

I create the project in STM32CubeMX, version 5.1.0.Select STM32F3-Discovery board.Delete USB and change HAL to LLClick "Generate Code" and the program hangs up. the screenshot and .ioc file is attached.How to learn the reason?

DOlov by Associate
  • 1198 Views
  • 1 replies
  • 0 kudos

STM32CubeMX 5.1.0 eclipse plugin to System regen failure

Using System Workbench 5.8 and 5.9 (both have same issue) with eclipse CubeMX plug in 5.1.0. Target device STM32L462RE. Library is STM32Cube FW_L4 V1.13.0. Initial project and code generation is fine. Launching STLINK-V2 works normally. When ma...