STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1560 Views
  • 0 replies
  • 2 kudos

Using .extSettings file

In the help document concerning .extSettings file the information is unclear.As I read it the Groups section is supposed to create/add directories and files.It does not. I have generated the project for SystemWorkbench and EWarm.I downloaded a test v...

STM32L433 DMA Issues - No Interrupt

Hello Community:What I am doing should be easy and straightforward, but the results are not. On this card (NUCLEO-L433) I am using CubeMX to do just one thing - set USART1 to transmit and receive, with only the receive set up for DMA. I set it up in ...

Resolved! LL_TIM_*() calls take too much time.

I am having a problem with a timer. I use CubeMX LL drivers, with basic time-base timer configuration.STM32L100RCT6, TIM6 and TIM7. Core Clock = 32MHz, PCLK1 (TIM6 and TIM7) = 32MHzPrescaller = 31, which should set timer to tick at 1us. ARR value is ...

0690X00000BvalaQAB.png

Generated code doesn't call HAL_NVIC_SetPriorityGrouping

BUG REPORT:Using STM32CubeIDE 1.1.0 with a new STM32F401VE project, under the CubeMX perspective, when I change the system core priority grouping, it correctly limits the range of values that I can enter for the interrupt pre-emption priority and sub...

Tom V by Associate
  • 1723 Views
  • 2 replies
  • 0 kudos